AXIS#.IL.FB
Description
Note: Internally the resolution of the current scale is calculated by the value of AXIS#.IPEAK
/ AXIS#.IL
"Instruction list"
This is a low-level language and resembles assembly.FBSCALEINTERNAL.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Arms |
|
Range |
± Axis peak current (AXIS#.IPEAK) |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL.FB | 0x500A | 0x1 | DINT | 1000:1 | - | RO | True |
| AXIS2.IL.FB | 0x510A | 0x1 | DINT | 1000:1 | - | RO | True |